Page 3 of the datasheet shows the Typical Application.
There are no values shown in the Typical Application picture for the following components:
Capacitor connected from pin 14 to pin 15.
Schottky diode connected from pin 15 to pin 1.
Diode connected from pin 15 to pin 13
Schottky diode connected from pin 13 to Ground.
There is are values or specifications given for these parts anywhere in the datasheet.
There are no instructions for selecting the 22uH inductor.
I have chosen VISHAY part number IHLP2020CZER220M11.
The VISHAY IHLP2020CZER220M11: Isat =1.7A, DCR(max) = 270mOhms, SRF = 10.7MHz
I have set the Current Limit for the TPS65233 to 600mA in my design.
Have I chosen a correct inductor for my design?