This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40050: TPS4005 abnormal issue

Part Number: TPS40050
Other Parts Discussed in Thread: TPS40055, TPS40057, LM25116, LM25117, LM25145, LM5145



Describe :  RKFF = 62K & RA = 430K that SMPS can normal work (Turn on point at 10V when ambient = 25 deg C)

issue :  The turn on point (UVLO) will change to 9.8V when ambient = -40 deg C

      Calculate the RKFF (55K ohm) and RA (443K ohm) for adjust the lower UVLO point (9.2V) , but it don’t helpful

      Could you please help reply it or tell us how to adjust it ?

      Thanks a lot.