This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to design a circuit based on BQ24650 IC for charging single cell Li-ION battery with maximum 2 amp.
The solar panel I will use has the following characteristics:
Voc = 7.2 v
Nominal Voltage = 6 v
Open Circuit Current = 1 A
For now, I'm using a work bench power supply set at 7 volt and 1 amp to simulate the solar panel.
I checked the voltage on all pins of the IC. Some are normal as indicates the datasheet but some seem strange i.e. the HIDRV pin.
here are the voltage value of all pins:
Could you please send the schematic again?
What is the end equipment/application for this?
REGN should be regulated at 6V. From your measurement, it is higher than your VCC. There is something wrong here. Have you tried to test on another IC?
hi Jing Zou;
thank you for your reply.
I have attached the schematic and the pcb layout. But just in case I attach them again.
Jing Zou said:What is the end equipment/application for this?
This will be a power bank charged with solar panel and simultaneously charge a phone via USB.
Jing Zou said:Have you tried to test on another IC?
No. I have not test the circuit with another IC. But before that, would you please verify the circuit and the values of the components (caps and resistors)?. If all other components are chosen correctly, I confidently can solder new IC and other components on another pcb.
Thank you again for your time.
best regards.