This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI sir
Test condituon1 : Vin = 19V, Vout= 24V , Iout = 1.5A
Test condituon2 : Vin = 26V, Vout= 24V , Iout = 2.6A
After test , The L, C become so hot. Any idea to slove this problem ?
Attached circuit came from WEBENCH, is OK or not ?