Hi
My Customer has question.
The customer says it can not be adopted unless the contents of the question clear.
Please give priority to this question and respond.
Customer's spec is as follows.
Vin =6V~17V
Vout=1V
Iout =2.4A
If there is a provision of Ton min, please tell me the value of min / typ / max.
The specification of datasheet P3 [tON] is understand to be On time under the test condition of [Vin = 12V / Vout = 1.05V].
In Figure 5, there is a graph of [inputVoltage vs outputVoltage].
This graph means that [Vin = 23 V / Vout = 1.05 V] can be outputted.
However, there is no provision of Ton min in the data sheet.
The customer wants to know if it is possible to output when Vin = 17 V / Vout = 1 V.
Best Regard
T Kishi