This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61086: TPS61086 Output Voltage

Part Number: TPS61086

Hi TI Experts,

I plan to use TPS61086.

Input Voltage: 3.0 to 4.2V (Supply from a Rechargeable Lithium Polymer battery)

Output Voltage: 6V

Current consumption: 500 ~ 550mA

At the datasheet, the Output Voltage is Vin+0.5V to 18.5V,

May I know the minimum value to Vin+0.5?

What is meant by Vin+0.5V?

Thanks,

Br,

Teach Me