Hi, Team
Would you help to check the BQ52122 setting as below:
1.What is default DC/DC output voltage for BQ25122?
2.Could we get temperature information from BQ25122? (read real temperature from external NTC by I2C)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team
Would you help to check the BQ52122 setting as below:
1.What is default DC/DC output voltage for BQ25122?
2.Could we get temperature information from BQ25122? (read real temperature from external NTC by I2C)
Ray,
1. The default output voltage is 1.2V for the VSYS.
2. The BQ25122 indicates faults only. It doesn't have an ADC built it but whenever the TS pin voltage is within thresholds of COLD or COOL or WARM or HOT, you will recieve a fault and the register will update accordingly.
thanks,
Gautham
Battery Charger Applications
Ray,
PMID will need the capacitor min as recommended by the datasheet.
LS/LDO is okay to float if not using.
/MR is okay to float as pulled up
LSCTRL is okay to float as pulled down internal
TS is not okay to float. I would recommend a resistor divider with a 60% of VIN.
Regards,
Gautham