I have read TPS65273V datasheet. As I understand it, when the output voltage is set with a resistive divider via FB pin, the output voltage can be up to 15V. But, when it is set via I2C, the VOUT pin is directly connected to the output node and therefore the voltage limited to 1.95V. Is it possible to connect VOUT pin to the output node through a resistive divider in order to reach voltages higer than 1.95V? I would like to use voltages in the 3.3 - 4 V range.
Thank you for you help