BQ2407x chargers specify that the maximum R_ILIM resistor value must not be larger than 8kOhm, which essentially sets a 200mA input current limit.
The charger though can obviously handle a smaller input limit (100mA) in USB mode (EN1=EN2=0). My question is, what are the consequences of exceeding the 8kOhm R_ILIM limit? Say, I set (EN2,EN1)=(1,0) and then I use 10.16kOhm (for 150mA) or 21,8kOhm (for 70mA) for the ILIM resistor. Would these configurations really not work or what negative consequences should I expect?
Thank you,
Karoly P.