Other Parts Discussed in Thread: TPS40170
I am currently designing a project where I need to supply and control Peltier modules. These require up to 10A with at 34V.
The plan is to use an LM5119 in dual channel mode with a pseudo H-bridge configuration (one side of the Peltier connects to VOUT1, the other side to VOUT2). This means that one of the channels at any given time will need to sink current. The question is, can the device sink this load current, will it be damaged, or will it go into protection mode? I see that page 18 of the datasheet states "the capability to sink current from the output in certain conditions such as light load, overvoltage, or prebias start-up.", but what is defined as light load?
Many thanks for your help.