HI Sir
I saw TI have two recommend surge protection circuit ,May I know below two circuit can support 2KV surge ?
So far we test 1.75KV surge ,VLNB pin of TPS65233-1 will damage
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Sir
I saw TI have two recommend surge protection circuit ,May I know below two circuit can support 2KV surge ?
So far we test 1.75KV surge ,VLNB pin of TPS65233-1 will damage
Thanks
Hi, Hsiao
The DT400(TVS) diode responsing is too slow to clamp the LNB_PWR0 voltage, so we must add a 1N4007 between DT400 and DT401 for the surge test, it can prevent high voltage pass to IC before DT400 clamp LNB_PWR0 voltage.
No need BOM.
Hi, Hsiao
Yes, the R1=1.5kohm is ok.
Suggest to use 0805 package and can bear at least 0.25W power resistor for R1.