This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072T: Question for BQ24072T 104AT Thermister Divider Resister

Part Number: BQ24072T

Hi 

I have very simple question for BQ24072T  . 

Our customer want to use  BQ24072T with 104AT (100k) thermister for TS setting. 

But I can not calculate matching resister for TS Divider ( Upper side / Lower Side ) resister .

Could you calculate for resister value this Customer spec?    

1)  Thermister  spec 

     TH03-4F104FD  Mitsubishi   

      Thermister .Spec 

         25 degree    100k  ohm

         10 degree  212.9k ohm  

         45 degree  40.8k ohm 

2)   Trip temperature 

        Cold Temp     =  10 degree 

  Hot  Temp      = 45  degree 

[ Question ]  

  Could you tell us external divider resister value  ??  

 

Sorry.. I can not found  best resister matching combination . 

Regard

March Jasper ( Japan Disty Sugimoto)