Other Parts Discussed in Thread: BQ20Z65-R1, BQ20Z65, BQ20Z60-R1, BQ24765, BQ25708
I am using a bq20z65-r1 based battery that has PEC enabled for the charge current/voltage broadcasts. Unfortunately this is not compatible with the bq24725A charge controller I currently have design into my system. The battery manufacturer is unwilling to disable PEC for us (why this option is buried in a private key protected area of the flash instead of exposed to the end user is beyond me), and I would like to use the broadcast feature to enable charging without processor intervention. The leaves my only option as replacing the bq24725A with another part.
Which part is the most similar to the bq24725A (in terms of application), but that also supports PEC?
Thanks