Other Parts Discussed in Thread: TEST2
Hi,
we use the BQ2084 for our batteries. In our current application we are having some trouble with low currents. The capacity from the gauge differs from the real capacity of the battery after some time.
So we are thinking of activating the midrange capacity correction. In the datasheet is the following table:
My first question is if the second row from the table should be "<VOC75 and RelativeStateOFCharge() > 87%"? Otherwise it makes no sense in my opinion?
In our applciation we have low currents (<1mA) for longer periods of time and some short periods with currents like 300mA. After some time there are major deviations from the real capacity. Because of this deviation, it is not possible to fully charge the battery because of the Maximum Overcharge value which is 300mAh in our battery.
Do you think the midrange correction will help us or is there another solution you would recommend?
Regards,
Christian