This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
could you please support with following issue I have with LM5165EVM-HD-P50A?
In the schematic I've modified R8 and R9 in order to reach a higher output current (see image below).
These are the values I used:
R8 = 47kOhm
R9 = 100kOhm
Based on my calculations, like this I expect to reach ca. 100mA of output current, but the board never goes above 65mA.
Can you please advise?
Thanks and best regards,
B