This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H160-Q1: Power and ground protection

Part Number: TPS4H160-Q1

Hi,

I'm designing a pcb which is supposed to generate 24V outputs controlled by a microcontroller. As those outputs go to external devices, I want to protect my circuit against external problems such as short circuits polarity inversion ... My question is about the isolation of the ground because I don't know if I'm suppose to have separated ground between my microcontroller and the power outputs and how to connect it each over with a diode or something else. Something else I think it's strange that there is no input capacitors.

Thanks