Other Parts Discussed in Thread: TPS63000
Dear suppormember,
I measured the output noise of TPS63000EVM.
I have a question about output noize at TPS63000EVM.
From measurement of spectrum analyzer
① It can be confirmed that it is growing at the time of down conversion
(high input voltage condition Vin=5.25V).
② It seems that the noise floor is rising at no load.
Q1.
What are the reasons for ①and ②?
Q2.
Switching noise extends to the 800 MHz band.
Is there countermeasure against noise in the 800MHz band?
I attached a waveform.
Could you check it?
<Specification condition>
Vin: 1.8 to 5.25 V
Vout: 3.8 V
Iout: 0 to 300 mA (max)
Best regard.
Bob Lee.