This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Here is the design that web bench designed, it suggests an LM5036 but this part does'nt exisit. Is this a typo? What woudl the part really be?
webench.ti.com/.../webench5.cgi
Hello Andrew,
In the Webench design you included in your inquiry, I see four main supplies and two LDOs.
These are:
TPS62143
TPS54427 which feeds LP5907
TPS62130 which feeds LP38841
TPS56720.
No LM5036 shown in any of these designs. Would you post the Webench schematic that shows the LM5036 please?
Regards,
~Leonard
Not sure what your looking at because none of those parts are in this design. Posted teh schematic and a pdf of the web bench design in the next posts. hope that clarifies.
Hi Andrew,
As it turns out, the LM5036 has not yet been released, but the Webench team got the model completed ahead of schedule and enabled it for Webench designs. The Webench model is being disabled until the LM5036 is actually released, so you could re-do your design now and use a currently available device. It looks like the LM5036 will be released mid-to-end of April, so you could wait until then to use the LM5036.
Apologies for the inconvenience and confusion.
~Leonard