Dear TI,
In D/S 8.3.7.4 Reverse-Current Protection.
I have the following questions.
1.Can I use method 1 only to achieve the protection function? (don't use method 2)
2.Comparison Method 1 and Method 2. Is the loss of diodes smaller in Method B?
3.Is using Diode=SK34 and Resistor=4.7K correct in Method 2?
Thank you
Best regards,
Ronald