hello.
I have a question about UC2843A.
Can you get a graph of frequency vs ICC?
It is currently under evaluation.
65kHz:Icc=21mA
100kHz:Icc=28mA
It is a result.
I want to know whether this value is normal.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello.
I have a question about UC2843A.
Can you get a graph of frequency vs ICC?
It is currently under evaluation.
65kHz:Icc=21mA
100kHz:Icc=28mA
It is a result.
I want to know whether this value is normal.
Thank you.
Hi Masazumi-san,
The current consumed by the IC is releated to the frequency of operation and to the capacitance of the mosfet that it is driving.
Can you share the datasheet for the mosfet?
Also since the UC2843A is a biploar device the bias current will be higher than the UCC CMOS based versions.
Regards
Peter
hello.
UC2843A is used for two kinds of circuits. One is NPN and PNP transistors
The totem pole driver (NPN and PNP transistor) is added to the outside to drive the MOS. , The other drives directly.
NPN:2SC2873
PNP:2SA1213
MOS:TK9A20DA
thank you.
hello.
I sent the FET data with the previous mail.
This time we will send the current UC 2843 A and FET composition. (Attachment)
Thank you.Microsoft PowerPoint - UC2843A.pdf