Dear support member,
My customer use LM22675.
I have a question about line reguration.
Daimen is a 3 phase power supply,
The input voltage fluctuates at intervals of 8 ms at 0.1 V.
The output voltage fluctuated at intervals of 8 ms at 50 mV.
Is this normal behavior of IC?
If it is not normal operation,would you teach me the reason?
Specification condition
Vin: 27 V
Vout: 5 V
Iout: 1A
Best regard.
Bob Lee