This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53219: Can TPS53219 meet VIn=12V, Vout=3.3V, output current=26.8A and OCP=33A?

Part Number: TPS53219
Other Parts Discussed in Thread: LM27403, TPS40303, , TPS53119

In datasheet, It describes that Wide Output Load Range: 0 A to > 20 A.

But it is a controller, can TPS53219 meet VIn=12V, Vout=3.3V, output current=26.8A and OCP=33A?

Is there any concern?