Other Parts Discussed in Thread: BQ2002
Hi
I am sorry for the many question. Our customer ask some question about the behavior of BQ2002D.
1. Is there any way to disable the timer? (disable the TM pin function.)
Because our customer would like to disable the timer and MCU will be disable the charging at the more than 440min instead of BQ2002D.
2.Regarding to Max temperature termination, it is mentioned on the datasheet as VTCO = 0.225 ∗ VCC ±5%.
However at figure 2 the formula is as VTS < 0.25 * VCC. Which is it correct? 0.25 or 0.225?
3. Our customer would like 2A fast charging using BQ2002 with NiMH. However 2A of the charging current is much high.
And we could not find the good solution.(The most of solution using BQ2002D is low current charging solutions with NiMH.)
Do you have any TI's solution for that? (the device is not only BQ2002D but also other device will be fine.)
Best Regards,
Koji Hamamoto