Hello,
My customer have two questions about TLC59208F below.
1. When the power supply is turned on, the voltage of VDD drops from 3.3 V to 2.5 V, is there a problem with IC?
Voltage drop time is about 20 to 30 ns.
2. About I2C Fast Mode(400kHz),
Fall time is state as min 20nS + 1Cb in the datasheet.
Its time will be 6 ns on their system. Should it be better to adjust to 20 ns or more with buffers?
Regards,
Taichi Nakamura