Other Parts Discussed in Thread: UC2610,
Hi
I have a question on figure 2
FORWARD CURRENT v.s VOLTAGE, the minimum current is 0.001A (1mA)
my design is the """ signal --- 5 k ---(diode cathode) (diode anode ) -- 5V """
I want to know
when signal level is 1V level , the pull up current is around 0.4mA. ?
is that mean diode is turn on ?
is this situation , what is the forward voltage @25 degree, 0.3V ?