There was a previous answer that the LM5032 can also be used with DC input.
How does the LM5032 operate when the input voltage of the LM5032 rises and exceeds the output voltage setting voltage DC 400V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There was a previous answer that the LM5032 can also be used with DC input.
How does the LM5032 operate when the input voltage of the LM5032 rises and exceeds the output voltage setting voltage DC 400V?
Hello michifuji,
The LM5032 is a dual interleaved PWM controller and the operation of the LM5032 in the situation you describe really depends on how the controller is configured.
For example in the datasheet the controller is configured in the forward topology.
This means that Vout = N*D*Vin so if the turns ratio (N) is greater than 1 then Vout can be greater or less than Vin by controlling the duty cycle from approx. 1 to very low values.
You can also get Vout to be less than or greater than Vin with a flyback topology.
400V is a very high output voltage. What is your application and what is your input voltage range ?
Regards
John
Thank you for your reply.
The input voltage is DC 150V - 800V.
Application is battery related.