This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® 도구 / LM5067 : UVLO / OVLO & SURGE Test

Part Number: LM5067
Other Parts Discussed in Thread: LM5017

Tool/software: WEBENCH® Design Tools

Hi!
Question about LM5067 surge test.
6V is applied to the UVP pin.
The OVP pin is connected to GND through a 10K resistor.
In this case ...
When the surge voltage was tested with a 5 KV impedance 2 ohm condition,
Gate voltage will be OFF-> ON.
Please tell me how to prevent it from turning OFF!
Also,
LM5017 IC is damaged during surge test. (Auxiliary power IC)
What should I do to prevent damage?

The surge test must meet the impedance 2 ohms condition at 20KV.
The input circuit has a surge protection circuit.
We will send the schematic and PCB data together.

Tell us how we can improve!

LM5067 & LM5017 Surge Test - 180622.pdfBM091M.pdf