Hello,
Please clarify my doubts related to TPS65266-1 regulator below:
1. How to control(Enable/Disable) Outputs of the DC-DC regulator: TPS65266-1 ??
2. Is there any possibility of getting a Switched voltage regulator with similar specifications as TPS65266-1(Rated current 2A(@3.5V) for at-least one regulator in the regulator) but with INPUT supply: Vin min= -ve to 3V, Vin max= 9V to 12.5V ??
Thanks in advance.