This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87322E-Q1: How to Adjust UVLO for LP87322E-Q1??

Part Number: LP87322E-Q1


Hello,

I have few queries on regarding LP87322E-Q1 UVLO set-up & schematics implementation, please clarify the following:

1. How to Adjust UVLO for LP87322E-Q1??

2. Programmable Output Voltage given in datasheet is: 0.7 V to 3.36 V

                   - My application requires 3.5V, is it possible to set it using external voltage divider circuitry?? If Yes, please let me know how the connections should be.

Thanks in advance.

  • Hi Madhu,

    > 1. How to Adjust UVLO for LP87322E-Q1??

    UVLO is a fixed level, 2.6V falling and 2.63V rising (typical). This is specified on the "PROTECTION FUNCTIONS" section of the electrical characteristics table.

    > 2. Programmable Output Voltage given in datasheet is: 0.7 V to 3.36 V
    > My application requires 3.5V, is it possible to set it using external voltage divider circuitry?? If Yes, please let me know how the connections should be.

    I would not recommend this. The device is validated and specified up to 3.36V. I am not sure that it will meet specification when operating at a higher voltage.

    Regards,
    Karl