Hello,
In my application, only one BQ76PL536 is connected to DSP28035, so it works as device to host mode.
I didn't change the address for BQ76PL536, so the address is 0, and the clock frequency was 250kHz.
I capture the SPI waveform and found that BQ76PL536 doesn't response any host's command:
For example, the waveform below shows the read IO register operation, the data is 0x00, 0x31, 0x01, 0x55(dumy write to keep CS and clock for 536 response 1 byte )
1: MOSI 2:CS 3: Clock 4: MISO
Any special setting to enable device to host mode?