This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using BQ24650 Ic for charging the 3.7V, 6600 mAh battery and the input supply form the solar panel is 12V, 30W. I want to charge the battery as well as want to supply the load circuit (Application circuit) of up to 4.2V, How can i make the circuit for this ?
I have changed the value of R2 which was 499k to 79.19k for 3.7V of battery (PFA). For the application circuit (from direct solar panel : Vsys) supply should i connect it to parallel to battery or connect a 4.2V LDO.
Regards