This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Last product SoC Problem

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: GPCRA0

Hello;

My cell is Kokam SLPB080085270 (6S1P). Battery features;

- Max Voltage = 4.2V

- Min Voltage = 2.7V

- Capacity = 27000 mAh

The learning Cycle is completed. But there are problems in the last product. After taking the golden image, IT_Enable is being done. 

Then the BMS is starting to be used. The SoC is resetting when the battery is about 17.5-18V.  The log that is received about the subject is below.  What is the problem in the last prouct? I think the problem is that the average current is not updated quickly during sudden current changes. 

BMS_LOG.xlsx