Question from my customer:
If the ISET1 Low-side resistor fails (open) - what would be the consequence?
The (valid) input voltage range for ISET is 2V, and it can safely accept a VREF voltage (3.3V)... But what will the bq24610 do when ISET is pulled up to VREF (the low-side resistor, R12 - in the EVM schematic, fig. 10, OPENS up)?
Thanks!