This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The customer design with BQ24610, when the battery is not connected, ISET1 and ISET2 waveforms are found to be abnormal, as shown in Figures 1 and 2.
When the battery is connected, the output battery voltage is abnormal in figure 3.
BAT output waveform as below:
ISET as below:
Please help check it.
Thanks
Star
Hello Star,
I have a few questions:
Can you provide the schematic?
What is the input voltage/current?
What is the battery voltage/Charge current?
ISET is an input, Is Vref abnormal? How are the vertical and horizontal set?
Best Regards,
Christian