This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS68470: How to Configure with Unused wLED?

Part Number: TPS68470

What do I do with the PMIC pins if I don't use the wLED boost converter?

  • 1. Connect wLED_SW node to GND.
    2. Float wLED output
    3. Float NTC temp sensors
    4. Float wLED drives
    5. Keep 3V3_VDD ball D1 connected and with input capacitor present

    If you are not using the wLEDs but want to use the boost converter as a voltage boost then, only do # 3 & 4.