This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
In designing my project, I was basing my design on a prior project that used a 3.3 V input voltage Vs and an appropriately sized shunt resistor Rs. Unfortunately, I hooked Vs to a 5 V input and exceeded the maximum specified current for the device for some minutes (which is 15 mA, according to the datasheet). However, I only exceeded it by 1 mA, so I haven't let out any magic smoke.
What is the expected behavior of a precision shunt like this if it's failed? Currently, I am obtaining 4.3 V across my output and ground, indicating to me that the LM4040 is doing something, though I'm not getting the desired 2.5 V.
Hi Albert,
Once a device is outside of its maximum specified current, it is in an unknown state and we cannot guarantee any mode of operation. If you are powering up the device and obtaining 4.3V, then the LM4040 is failing to regulate to its desired 2.5 volts.
The device does not necessary need to produce any smoke to show that it is failing. As you can see, the wrong output voltage indicates that the device is damaged due to exceeding its maximum specifications.
Hope this helps,
Ethan