Other Parts Discussed in Thread: TPS1H000-Q1, TPL7407LA
Hi TI Experts,
I plan to use TPS22810 as load switch to drive a relay for power supply sequences.
Can TPS22810 able to drive an inductive relay?
The load relay characteristic as below:
44 mH @ 100 Hz
Rshunt 37 Ohms @ 1 kHz
26 mH @ 1 kHz
Rsh 109 Ohms @ 1 kHz
DC current when energized 350 mA
In the mean time, i need to know whether flyback diode is needed or not, or I can use the quick discharge portion to de-energize the coil.
Thanks,
Br,
Teach Me