This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are planning to use BQ25600 PMIC in one of our battery operated vibration sensor .
we are in doubt about vibration acceptance of BGA package of BQ25600, ( vibration will goes up to 16g continuously).
please confirm ,
if BQ25600 is not the part number used for vibrating condition please suggest alternate part number with SHIP mode ,option .
Battery details are mentioning below.
1. Nominal voltage. : 3.7V
2. Nominal capacity. : 4.4AH
3. Full Discharge voltage (min). : 3.0V
4. Full charge voltage (max). : 4.20V
5. Constant Discharging current (max) : 1.1A
Hi James:
The battery voltage is programmable in REG04. But we do not have ADC in bq25601 to customers to read the data. bq25895 build in ADC, you can look up the datasheet.