Other Parts Discussed in Thread: TPS22810
Hi,
I'm currently working with a circuit with multiple TPS22958Ns which are connected in cascade;
The circuit is shown below.
The problem is, when VBIAS is 5V, whether ON is low or high,
the resistance between VOUT and GND (for both TPS22958) is 68 ohm, which is not what I expected.
Due to this resistance, power dissipation is happening.
In function block diagram, TPS22958 has MOSFET between VOUT-GND, but it says it is not featured in the TPS22958N,
So my question is...
1. Is it normal to have 68 ohm of resistance between VOUT and GND?
2. How can I cut the linkage between VOUT and GND?
3. I am planning to replace TPS22958 to TPS22810. Will TPS 22810 have the same problem?