Hi Team,
we have been using the BQ24031RHLR for a previous project and it worked fine on many 100k units.
Now with our new design we experienced on some boards that the power manager got damaged after production. The chip consumes around 230mA without any battery or load attached. In this case the chip is supplied with 5V from AC pin. The chip still provides 5V at the output pins but gets really hot. The /ACPG pin which is a open drain output remains at 200mV with a pull-up of 100k to 3.3V.
The package marking says:
BZJ
TI 33k
C6E5
From the datasheet I could not tell what the second and third line means and how to translate it to a batch number or production week/year.
After having replaced the chip with a new sample everything worked fine.
The USB and the LDO pin are the only pins that are not connected on the board and theoretically the chip could have been damaged by ESD but this is only a theory.
Was wondering if you have a similar case with any other customer? Could it be related to this specific production batch?
thank you in advance
/Mathias