This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2587: Isolation between Input & Output voltage levels

Part Number: LM2587
Other Parts Discussed in Thread: LM3478, UCC28711, LM1084

Hi,

I am trying to find a controller for flyback buck converter to convert 24VDC to 5VDC. I came across LM2587 on the way.

1. If we design using this controller and the transformer to convert from 24VDC to 5V DC,8A, do we get isolation between input side and the output side...?? please clarify.

2. Please suggest a controller for isolated DC-DC converter. Input voltage 24VDC & output voltage levels : 5V,8A; +15V,2.2A; -15V,1A requirement.

Thanks

Vishnu