Hi,
We got a question from the customer about LM3410.
Could you help us?
[Question]
They evaluated this IC by EVM. So they have three question. Please refer to the attached file for details.
LM3410EVM Inductor Current_Aug2118.pptx
1. The inductor current overshoot occurs at the rising edge of DIM signal. It seems to be big as increasing the output capacitor. Therefore I assume the inrush current causes this phenomenon. Is this my understanding correct? If there are other solution except for decreasing the output capacitor, please give us the solution.
2. When the input voltage is 4V, the inductor current reaches the current limit and the big ringing occurs. Are there any solution for improving the stability?
3. Could you provide an information of the best IC under the following condition?
Vin=4~7.2V
Vf=11V typ
ILED=350mA
Dinimmg=Analog or PWM
Best Regards,
tateo