Other Parts Discussed in Thread: LM3410
Hi,
I want to drive a set of 4x high power LEDs at about 700mA (one at a time at i2c configurable current) using power from a single lithium cell (3.7V).
The LM3643 and LM3643b each driving two LEDs look like a great candidate when used in Flash mode. Our current LED driver also has a flash and a torch input and we are able to use the higher current so long as the device is within acceptable temperature ranges.
Is there a way to force the torch mode to not time-out?
(That is to bypass / ignore the settings in SNVS967A - 9.6.8 Timing Configuration Register (0x08) )
Alternatively- I'd be happy for recommendations of LED drivers that might achieve what I need without the time-out pain.