Other Parts Discussed in Thread: BQ24163, BQ24193, BQ24650
Hi there
Very interested in using the BQ25895 IC to solve a couple of problems. I am trying to understand what is possible with this, so I have the following hypothetical questions:
1/ With BATFET being controllable via I2C, if this is switched off via I2C but Vbus is still powered, does the IC provide a regulated supply on VSYS still? Similar to how it would behave if no battery where connected (even though it actually is - but forced so it won't battery supplement).
2/ If I had a large supercapacitor on SYS that was pre-charged to a level above the minimum SYS voltage and VBUS not connected, I assume BATFET will be switched off? Would the IC use any significant current?
3/ Not related to the above two questions: Quiescent current: I assume that with VBUS unconnected and simply a charged battery present on BAT whilst no current is being drawn on SYS, then quiescent current should be < 60uA?
Thank you in advance.