Other Parts Discussed in Thread: PMP9774,
Hello,
I have an application where we're using the TPS61088 to drive a motor. Input is 3 'C' cells, nominal voltage from 4.6V down to 3.6V. Motor voltage is 6V. I'd like to be able to vary the motor voltage from 4.5V to 6V. Is it better to use a digital potentiometer on the high side resistor of the FB pin, or would be be better to inject a DC voltage like the PMP9774 reference design? Rate of change is slow, like changing the value once per second.
Thanks,
Derek