This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
I have the following schematic above represented.
It in the DC input supports between 4.35 to 16V.
I vary the input voltage and the current consumption is maintained so the power consumed increases with the voltage. For instance with 5V the PCB consumes 10mA and with 10V consumes the same 10mA.
Can anyone clarify why this happens ?