Other Parts Discussed in Thread: TINA-TI, LMZ31710, LMZ23608
Is it possible to run multiple LMZ14203H devices in parallel for higher output current operation? Perhaps through 0.01ohm ballast resistors? If so, would you connect all the Ron pins together and use a single resistor to set the switching frequencies of all LMZ14203H's identically? Would you connect all the FB pins together and use two resistors off the first LMZ14203H to set the output voltage (essentially making it a "master" and the other devices "slaves")? I downloaded the Tina-TI spice software in hopes of simulating this, but the LMZ14203H device is not available in the software anywhere that I could find. Any help would be appreciated, thanks.