This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer hope to get schematic / BOM / and efficiency data for Flyback solution (It is OK to except UCC28730).
Request spec is below;
If there any matched data, please give these data.
・Vin: AC 85V~265V
・Vout: DC 14.5V / 40W (2.76A)
・Non-Isolated solution, they want to use large inductor, not transformer.
・Required efficiency: 85% @ 100mA and 92% @ 2.76A
・In the case of not to use UCC24650 and SR controller (UCC24612, etc).
Best regards,
Satoshi