This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180: Transformer compatibility

Part Number: LM5180


Hi,

My customer wants to use LM5180 for a power adapter.

  • Vin 24VDC
  • Vout 15VDC
  • Iout 250mA

He was wondering if 750315490 transformer (50uH, 1.4A saturation current, 1:1 turn ratio)  is compatible with LM5180. Is there something to worry about while selecting transformers?
How much should the minimum base load be?

Thanks,
Needhu