This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24100: Not charging battery.

Part Number: BQ24100

Hi everyone!

I have a problem.

When the input voltage is + 5V, the battery does not charge
When the input voltage is less than + 5V, the battery is charged.

I take schematic from datasheet (calculate only resistor on SET1 and SET2 pins (1.5A current)), but it doesn't work.

My scheme:

V input= 5V. Only one 18650 battery.